This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951-Q1: Is it suitable for the full bridge secondary?

Part Number: UCC28951-Q1
Other Parts Discussed in Thread: UCC2895, UCC28951

Hi, I plan to design a 3.3kW charger with an output voltage range of 54 to 90V and an input voltage range of 380 to 420. As the maximum output current is 40A  and if I use a centre-tapped secondary in the PSFB stage, the voltage stress across the MOSFET is high and so is the cost. Can I use full-bridge config at the secondary side of PSFB and if so can you provide any reference for the same?