Hi,
Efuse in our design is shut down immediately when its input of 12 volts falls below 10.8 volts. We are expecting the under-voltage shutdown to happen only after 12V falls below 4.5V.
In the datasheet, we have noticed the UV thresholds for the following pins: VDD and VIN: 10.8V (default; can be rewritten through PMBUS access) and 4.22V, respectively.
We have on board resistor divider R1=12.1K and R2=4.7K to set the UVLO threshold @ 4.5V.
We tried even after changing the VIN_UV_FLT register value to 0x38 (4.32V) instead of 0x8D (10.8V), but the issue still persists. Please assist us in resolving this matter as soon as possible.
Thanks,
Veeramanikandan