Hi, regarding the current limit settings, I have some questions, please advise.
- what's the behavior of the TPS2111 when loading exceeds the current limit? Switched off output or maintain max. current avaiable (1.5A)?
- If I set the RILIM to 300ohm, then the current limit per datasheet calculation is 500/300=1.66A typ. Then what is the tolerance under this setting? Datasheet only give the tolerance with RILIM 400ohm and 700ohm, I want to know the accuracy with 300ohm.
- If RILIM is 300ohm, does 1.66A typ. take effect? Or the max. current can provide is still 1.5A?