This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The customer design the schematic with BQ24610 for 4 series battery. during charge they plug in and out the battery, BQ24610, HIDRV MOS, LODRV MOS damage.
Attached the schematic for your reference.
Hot plug the battery why the BQ24610, HIDRV MOS, LODRV MOS will damage?
Waiting for your reply.
Thanks
Star
Hi Star,
It is likely the damage is caused by the inrush current and voltage spike when performing the hot plug.
Can you provide a capture of VBAT1 and PH (on the same capture) when battery is plugged in?
It seems like your customer is not using the /BATDRV and there is no system load based on the schematic, is that correct?
Regards.