Hello,
I am an FAE for a distributor that handles TI products.
I received a question from a customer about parallel connection with LM5177.
I found out in the thread below that this device can be connected in parallel.
(Question 1)
Since the image of the circuit attached to the thread is rough, details cannot be confirmed.
Is it possible to provide me with a document that clearly shows the details?
(Question 2)
Is it possible for the circuit attached to the thread to pass the current equally between the two devices?
If possible, please tell me how to make the current flow evenly.
(Question 3)
When paralleling, should the out-of-phase clock be input to the SYNC pin?
(Question 4)
Please let me know if there is a clock generator that can be used when connected in parallel. Output should be 4 or more.
Specifications are below.
VIN: 19V to 30V
VOUT: 24V
IOUT: 15A
Best regards,