Other Parts Discussed in Thread: UCC24612, UCC27714
Hi, as I am designing a 3.3kW PSFB for a 72V battery charger with the following specifications, Vin=380 to 420V, Vout=54 to 90V, Iout max=40A, 3.3kW. As the secondary side voltage stress seen by MOSFET in centre tapped configuration is high so, the overall cost is going high. I am planning to use the full bridge configuration on the secondary side with the UCC24612 gate driver for individual MOSFET, I will not use OUTE,OUTF of UCC28951. I wanted to know whether it will work or not and what will be the effect on the efficiency of the converter.