Greetings,
For the TPS7B4253 Input voltage will be between 6.3 - 7.7V, and the corresponding output voltage between 4.5 - 5.5V.
With this output I would like to provide supply to an sensor IC that requires 5V nominal supply. The output of this sensor IC is ratiometric.

I will scale down to input voltage by R1 = 4k, R2=10k resistors.
Then I will raise the output voltage of the sensor IC again by using OP-AMP. For this purpose I want to use this voltage tracker LDO. Is it okay?
The output of the whole circuit should be ratiometric even up to 7.7V.
For scaling down I did not choose an OP-AMP because of the capacitors in supply of sensor IC.
Is this configuration okay or do you have any other solutions or recommendations?