Hello, I'm writing to ask you something about LMG3422R030 module's VI characteristic and thermal characteristic.
In the file which name is "LMG342xR030 600-V 30-mΩ GaN FET With Integrated Driver", Datasheet,
There is no information about VDS - IDS characteristic curve, RDS(on) - IDS characteristic curve.
I need the information of these characteristic to estimating junction temperature with power loss(conduction loss + switching loss)
how can I get these information? or there is another way to carry out junction temerature estimation?
and, about thermal characteristic, I want to get some information about RC thermal network's R,C values.
In the datasheet, Thermal information is already existed, but to estimate the junction temperature of GaN HEMT, I need Cauer or Foster network constant value.
if there are some ways to get information, plz tell me.
In addition, LMG3422R030 module consists of Normally-ON GaN HEMT and Si-MOSFET.
If there is no information that I mentioned, Please tell me the model name of GaN HEMT and Si-MOSFET that make up LMG3422R030.
Thank you for reading.