Hi
How can I configure the bq78PL114 when I want to use only 2 temp sensors for the cell stack instead of all 8 sensors.
We use the bq78PL114EVM for our first steps.
After calibration procedure of temperature, all values are ok in the case that only 2 sensors are connected on the EVM.
But, if I connect a load and a high current about 2-4Amps is flowing trough the EVM-Board, the temperature of cell3-8 rises above 50°C in a short time,
the two channels with connected sensors (Cell1 and Cell2) shows still the correct temperature.
Can I modify something, hardware or configurations in the Wizzard to solve this problem?
We use the firmware FW4452 because the BMS-Design should have 5mOhm Rsense and I only have the possibility of 1, 3, 10mOhm with the
newer firmware FW5000.
Thanks and regards
Dietmar