部品番号: TPS628512
データシートを見ています。
図 10.43 の出力電圧リップルで Vin=3.3V、Vout=1.2V の時のリップル範囲を教えてください。
チャットでの回答が得られず、ここで質問するように言われました。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
部品番号: TPS628512
データシートを見ています。
図 10.43 の出力電圧リップルで Vin=3.3V、Vout=1.2V の時のリップル範囲を教えてください。
チャットでの回答が得られず、ここで質問するように言われました。
Hi,
Can you please post your question in English?
Best regards,
Varun
I'm looking at the datasheet.
Please let me know the ripple range when Vin=3.3V, Vout=1.2V in the output voltage ripple of Fig. 10.43.
I didn't get an answer on chat and was told to ask here.
Hi,
Output ripple is dependent on the amount of output caps and parasitic of these caps. You can configure the BOM using our WEBENCH tool and check the expected ripple: https://webench.ti.com/power-designer/
I've attached an example design with COUT = 2 × 22uF and the ripple was 1.21mV for 2A load.
Best regards,
Varun
Mine uses two 10uF capacitors.
Please tell me the range of ripple value.
ex.
20mV~30mV
Hi,
The ripple is 2.53mV for 0 to 2A in FPWM mode and 37.52mV in PFM mode with COUT = 2 × 10uF.
Best regards,
Varun