Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO
We used the logic analyzer to grab the current data of BQ76952, and did not read any data actually loaded by 0.5A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
From your Excel file, it looks like after giving the 0x3A direct command, you are receiving a current reading of 0x00 43 00. This is in little endian format and corresponds to 0x43 00.

This is 17,152 in decimal format, or 17.152 A of current.
To help determine exactly what your problem is, I will need some more information.

For more information on BQStudio and I2C communication with the BQ76952, please see the Software Development Guide linked here: BQ769x2 Software Development Guide (Rev. B) (ti.com).
Best,
Andria