Hi team,
For the delay time calculation, in the datasheet, it says use td=Ct[nF]/175 + 0.5x10^(-3)

By using the equation, for Ct=100pF
td=100pF/175+0.5x10^(-3)=1.071429[ms]
But in the datasheet, the typical value for Ct=100pF is td=1.25[ms] (min 0.75[ms] and max 1.75[ms])
The question is:
- Why does the value differs? (calculation result: 1.071429 and typ: 1.25)
- What is the min, typ, max value for the "175" & "0.5" in the calculation fomula?
Regards,
Ohashi