Dear TI,
Could you recommend a part / approach to build relatively simple LED driver with up to 55V 20A or 85V 12A at least? Efficiency is not a concern, around 85% or higher would be enough, EMI issues is also not a concern for this design.
Input voltage is a two-option (not simultaneously):
* 21-25V
OR
* 42-50V