Part Number: LM5180
Hi experts,
Customers want to use LM5180 to generate multiple outputs, as shown in the figure below.
May I ask whether the 12V in the picture can achieve the 1.5% accuracy in the datasheet?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5180
Hi experts,
Customers want to use LM5180 to generate multiple outputs, as shown in the figure below.
May I ask whether the 12V in the picture can achieve the 1.5% accuracy in the datasheet?

HI
LM5180 can support multi rails, but as it sense the main winding voltage , 12V 0.3A rail regulation will be impact by the other two rails’ load. And it is also related to transformer’s leakage inductance and the dummy load adding at each rail. So it is hard to predict , but it will be challenge for meet +-1.5% regulations.
Thanks