Other Parts Discussed in Thread: UCC256403
The frequency at which burst mode occurs, is 350kHz.
Can this be lowered to 240kHz, as an example?
(Burst mode will only happen at no-load to prevent the output voltage from running away due to leakage energy).