This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3410-HB-EVM: Fault pull low

Part Number: LMG3410-HB-EVM
Other Parts Discussed in Thread: UCD3138, ISO7831

Hi Team,

Customers are using the LMG3410-HB-EVM for testing at LLC on several of their products. 

Currently, the two SN6505 on the EVM are removed, and the 3.3V on the secondary side provides power to pin1 of the ISO7831 and UCD3138; the GaN VDD on the primary side is provided by the 12V auxiliary power.

According to the user manual, U3, U4, and R2 have been removed and R1, R18, and D1 have been added.

It is found that once the Low side Gate is switched, the U2 fault pin signal will be pulled low, causing the high side gate to fail to work, and there is no 12V output.

However, if the SN6505 is used as an isolated power supply, the above problems will not occur.

Confirm that Vdd 12V and 3.3V are stable, and the first rule out the problem of UVLO. Could OCP cause it?

You can refer to the following waveforms

CH1: U2 pin5
CH3: U2 Pin4 Low side from UCD3138
CH4: Low side gate current

CH1: U2 pin5
CH3: U2 Pin4 Low side from UCD3138
You can see the fault pull low when the gate begins switching

  • Hello,

    Thank you for reaching out. Our team is currently out of office until January 3rd due to the winter holiday. Please allow us to respond after this time.

    Regards,

    Zach

  • Thanks for your patience,

    Using a bootstrap supply is known to have potential problems with stability, there is a chance that OCP could cause the fault but more likely is the VDD supply for high and low side GaN devices hitting a UVLO like you mentioned. Could you send me a waveform picture of pin 27 (VDD) for the high and low side GaN FETs during switching to check for UVLO? Also, are you using our LMG34XX-BB-EVM with 3.3 V gate logic?

    Regards,

    Zach