Other Parts Discussed in Thread: TL081, PMP9622, PMP8740
Hello,
I am using UCC3895 in a Full bridge converter 48V DC input, 320V DC output.
I want to insert a current regulator on the output with a shunt placed in series on the +320V output.
The regulation is made with a TL081 in differential mode on the shunt.
On which input of the UCC3895 to connect to perform this regulation without STOPPING the converter.
Thank you for your return