Other Parts Discussed in Thread: LM5156, LM5157, LM5155
Hi
Please introduce a solution that satisfies the specifications below.
-SPEC-
Input: DC 3.3V~7V ( Battery)
Output: DC 100V 0.001A
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Thanks for reaching out. You might want to use the LM5156 or LM5157 for example in Flyback configuration or as a boost + charge pump on the switch node ( please refer to the applications section of the datasheet for further examples). Let us know if you need further help.
Kind regards,
EM
Hi David,
You may find boost + voltage tripler application in LM5155 datasheet.

Best Regards,
Feng Ji