We encountered a problem, when the bq25792 in fast charging state is set before the host is shut down, and a larger charging current is set. Then host is shut down at this time, the bq25792 cannot automatically shut down itself after being fully charged, so the leakage current keep relatively large while system power off because bq25792 still runing.
If we do not make settings before shutdown and use the default charging current, the leakage current is smal after the bq25792 is fully chargedl. The problem is that the charging current cannot meet the design requirements.
We want larger charing current for example 2A while system off for short charing time, smaller charging current ( < 1A or even smaller) whlie host is runing depedent on the system temperature.