Part Number: TLC59482
Other Parts Discussed in Thread: LP5012, TLC59108, TLC59116
Hello Expert,
Do you have a reference source code for this device?
If yes, could you please share?
Best regards,
MIchael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ives,
I need your support asap.
I want to input to the HALF BRIDGE GATE DRIVER using the output PWM of the TLC59482.
And want to output 50KHZ using GRAYSCALE (GS) FUNCTION (PWM CONTROL).
Now output is 100Hz.
Could you please send guide how to set it.
Best regards,
Michael
Hi Michael,
If you want to use the TLC59482 to produce 50kHz output PWM signal, then you need to set f_GSCLK = f_PWM * 512 = 50kHz * 512 = 25.6MHz.
BR,
Steven
Hi Steven,
Thanks for your kind support.
Our customer can't support 25.6MHz from MCU.
Is there any way to output 50khz by multiplying or distributing inside this device?
or
Is there no way to make 50khz output except GSCLK input?
Best regards,
Michael
Hi Michael,
For TLC59482, the 25.6MHz GSCLK is a must.
We have other devices that supports internal GSCLK generation like TLC59116 / TLC59108, but they only support 97-kHz fixed PWM output signal.
BR,
Steven