This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: About EN_SHIP_DCHG function

Part Number: BQ25730


Hi,

I'm not very clear about the function of 'EN_SHIP_DCHG'.  When to use it or what's the use case of this bit? May someone explain more?

Thanks.

  • Hi Diverger,

    The engineer who supports this IC is out until Jan 3rd or later.  I will notify him of this post but I recommend that you also respond back to this thread on Jan 3rd.

    Regards,

    Jeff

  • Hi Jeff,

    Are there anyone can answer my question now?

  • Hi Diverger,

    Thanks for your patience. The user case is, when the end equipment is built and put on the shelf. We would like to enable the battery ship mode, so the battery won't be discharged after a long period of shelf time, for example months. 

    To wake up the battery in ship mode, the charger will charge up the VBAT to a pre-determined voltage. 

    To avoid waking up the battery in ship mode, the charger will discharge the battery cap to ground or a low voltage, provided the battery is in ship mode, by setting EN_SHIP_DSG =1. 

    Hope this helps. 

    Regards,

    Tiger

  • Hi,

    What do you mean 'battery cap'? This is what confused me. If it means a capacitor connected to the battery, then how to discharge the capacitor without discharging the battery? Or it means disable the battery FET then discharge the cap?

    Thanks.

  • It first needs to disable the battery FET (inside the battery), then discharge the cap outside the battery.