Hello,
I am developing a product that needs to be powered with 2 watts of power through the single usb-c port of a mobile device (Ipad, iPhone, Android,...) and receive USB 2.0 data from this same usb-c port of the mobile device.
Since the mobile device only has one usb-c port my product must have a second usb-c port to charge the mobile device connect to the first usb-c port.
I would like to use USB PD and USB BC 1.2 technology.
I think the TPS65988DH dual usb PD controller is most suitable for my use.
Is it possible to use it without flashing and autonomously:
without external controller (neither I2C, nor SPI, nor GPIO), without external power supply other than one of the two usb-c ports, simply by shorting PP_HV1 and PP_HV2 ?
What value should the resistor divider be placed at pin ADCIN1 and ADCIN2 for this standalone use?
Thanks for your help.
And a happy New year!
Etienne