This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS568215: Power supply design guidlines

Part Number: TPS568215

PFA, One of my load device is asking for the below requirement.

But normal power consumption will be 78mA only. How to take care about this while designing a switcher.

  • Hi Anusha,

    I'm confused about the question.

    Is that a process here that our TPS568215 power on/reset, or our load power on/reset but the regulator remains online?

    Do you mean the load current is a pulse changing between 250mA and 78mA?

    What're the circuit parameters like the range of output voltage?

    If our TPS568215 remains power on during the time pulses, I don't think there would be any risk since the load transient is only 250mA max and the output voltage can support the transient. So just design the regulator as normal.

  • Hi

    Im asking in general..  For any load asking for 250mA for initial 500us , after 500us it consumes 78mA only.

    How to take care about this requirement..

  • Hi Anusha,

    Then I think a normal design is sufficient for this application without a special design or taking care.