Part Number: LM5176

We are using LM5176 IC in order to supply TAS5768 power amplifier. We made the design in order it can be operated at 15,3V output levels.
Our input may be in a range 11 to 14 Volts and 24 to 27 Volts and unwanted level of 7-7.5Volts. So our amplifier design with LM5176 must
handle all above input source cases.
11 to 14 Volts and 24 to 27 Volts input source is OK. It works as expected. I can draw more than 5A current at 15.3V output. However, with 7V-7.5V input supply, I can draw no more than 1.9A continuous current at 15,3V output. I would expect to get at least 4-5A current at 7V input as well.
Attached is our design. What is wrong with it? Waiting your recommendation if any. Thanks a lot.