Part Number: TPS61087
Hi,
I have to design a Boost converter for 650kHz.
Required Specifications are listed below.
Input Voltage range is 2.7-4.2
Nominal 3.7V
Output Voltage 12V
Current 367mA
The Boost design in datasheet shows an inductance value of 6.8uH for 650kHz, but what I received from webench is 8.2uH. I would like to know whether this is fine or not. I am hereby attaching the link of the design that got from webench.
https://drive.google.com/file/d/18xe_UkyAmkRJwj98JC7pOj8MbKRj28MU/view?usp=share_link
Kindly check.
Thank you.