Part Number: LM22676
Other Parts Discussed in Thread: LP38852
Dear TI,
Is there possibility to get thermal characterization parameter (psi JT) to LM22676?
I tried to find this info in datasheet but without success.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I found only general information... that "For plastic packages, ΨJT is typically 0.5°C/W–2°C/W".
General information is not always accurate.
For similar package /PowerPAD/DDA/8 - ΨJT can be more than 2°C/W". It's 9.6°C/W
e2e.ti.com/.../lp38852-psi-jt-and-psi-jb
So that's why I'm looking for more precise information for LM22676.
Thank you for you detail and update,looks this data meet calculation and webench result.
hi,
I haven't find a document or information for LM22676 , the ΨJT is almost same for same package ,but also have related to die size,
recommend to use around 8 to 10 °C/W .
Elena