This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS746: Replace a part for TPS74601PBDRVR

Part Number: TPS746
Other Parts Discussed in Thread: TLV759P, TPS745

Dear Ti,

I want to know replacement part for TPS74601PBDRVR.

  • Hello, 

    Depending on what you would like there are a couple of alternative options. The TLV75901PDRVR is one option it is similar to the TPS746, but does not have a power good pin. Both parts are in WSON packages with similar pin outs pin 5 would need to be reconnected as it is DNC (do not connect) on the TLV759 and a PG on the TPS746. 

    If you want something similar but with a smaller Iout current range the TPS74501PDRVR is a good option and alternative to the TPS746. 

      TPS746 TLV759P TPS745
    AEC Q100 NO NO NO
    Output Options Adjustable Output Adjustable Output Adjustable Output
    Iout (Max) (A) 1 1 0.5
    Vin (Max) (V) 6 6 6
    Vin (Min) (V) 1.5 1.5 1.5
    Vout (Max) (V) 5.5 5.5 5.5
    Vout (Min) (V) 0.55 0.55 0.55
    Fixed Output Options (V) - - -
    Enable YES YES YES
    Power Good YES NO YES
    Output Capacitor Type Ceramic Ceramic Ceramic
    PSRR @ 100KHz (dB) 45 45 45
    Noise (uVrms) 53 53 53
    Accuracy (%) 1 1 1
    Vdo (Typ) (mV) 190 190 95
    Iq (Typ) (mA) 0.025 0.025 0.025
    Thermal Resistance θJA (°C/W) 80 80 80
    Min Package Area (mm2) 4 4 4
    Package Type WSON WSON WSON

    Best, 

    McKyla