This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6593EVM: Cannot find driver for USBSER

Part Number: TPS6593EVM
Other Parts Discussed in Thread: UNIFLASH

Hello

We have an eval board which we cannot communicate with.

The problem is that  we don't have a valid COM port until the usbser device driver is not properly installed on windows.

I find the driver files on local computer but it contains only two device address and the following which would be needed is not part of the list:

Vid_0400&Pid_2014&MI_04

I have the gcruntime v11 and uniflash 8.1.1 installed on my PC. Can you send driver or download link?