This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51215A: Output with TPS51215A VID0 and VID1 set low

Guru 12020 points
Part Number: TPS51215A

Hi,

I downloaded the PSpice Transient Model and am trying Sim.
I thought that if the V0pin of the TPS51215A was set to a voltage other than 0V and the VID0pin and VID1pin were set to Low, a voltage other than 0V would be output to Vout.
With the TPS51215A PSpice Transient Model, when V0pin was set to a voltage other than 0V and VID0pin and VID1pin were set to Low and SIm was executed, 0V was output to Vout.
Is this a specification issue of the PSpice Transient Model?
Or does the TPS51215A actually behave like this?

Thanks,

Astro