Other Parts Discussed in Thread: UCC28951, UCC2895, TL431
Hello,
i want to charge a 12V battery from another 12V battery via an isolated DCDC-converter. I need high efficiency at 500W and therefore i want to use the Phase shifted topology.
The input voltage varies from 11V to 16V. Is the UCC28951-Q1 sutible for such an application? Theoretically the use of GaN-FETs would be possible with the right gate drivers, isn´t it?
Thanks in advance and kind regards.