Dear Team,
At present, according to the table provided by TI's official website, the RT1/RT2/RTH resistance value should be calculated, combined with the actual output value of VREGN, it is found that the read temperature will fall at about 45 degrees Celsius, which is consistent with the actual temperature and table calculation (25 degrees) there is a gap, so in the part of the base value (ring temperature), which parts need to be adjusted?

In addition, the NTC specifications inside the battery are attached as follows:

Many Thanks,
Jimmy