Other Parts Discussed in Thread: TL1963A, TLV767-Q1
Hi
The smart door lock project requires low-power LDO, please help to recommend the following selection, thank you!
The main parameter requirements are as follows:
1. Static power consumption: not more than 2Ua.
2. Input voltage: above 8V.
3. Output current: 1A.
4. Output voltage: 3.3V fixed or adjustable.
5. Vdrop is less than 900mV
Regards,
Charlie