Other Parts Discussed in Thread: LMR62014, , TPS61040
Hello,
I am using the LM2735XMF to boost from 3.6V to 5V and 200mA in a battery powered design which has to achieve around 10 uA in low power mode.
The problem I am facing is that I am seeing an extra 90 uA current consumption that I have realized is coming from the FB circuit of the converter through Rfbt(R2) & Rfbb (R1) resistors.
Is there an easy way to avoid this current from draining the battery by modifying the circuit? I tested incresing resistors value but then the converter didn't work properly, so I assume it has to remain with similar values to the suggested by Power Designer (R2 = 10k suggested by the datasheet).
If it is not possible can anyone suggest a device that could fit our requirements with a simillar package (SOT23)?
Thanks