Hello,
I am interested if there is any way to prevent a TPS659XX system from powering up until the power button is pressed? We have a situation where a charger wants to trickle charge a dead battery and if we try to power up during this state, the charger things the battery cells are shorted. It seems the STARTON_VBAT bit would help us there, but it defaults to high, and must be programmed by software. However, in a dead system, we can't run software. I tried holding PWRON and RESPWRON low, and in this case the system draws up to 140mA, and then settles at 37mA, so this won't work either. We are trying to avoid having to manage the entire power path, but its looking like we might have to.
Thanks,
Cliff