Other Parts Discussed in Thread: PTH12040W, TIDA-00582
We are considering using two PTH08T250W in parallel for the purpose of controlling load current rather than load voltage by having external circuitry that senses the load current and drives the 'Vo adj' pin (of the master) with analog control function that has one of the inputs the difference between measured load current and the required load current. Has this been tried with PTH08T250W? Would this use of the device be recommended?
(We bought a board from a 3rd party that preforms this function but is using two pth1204w in parallel.)