Other Parts Discussed in Thread: BQ25730, TPS25750, LM5155, LM5156
Hi TI experts,
I am designing a device that run off a 5 to 6 cells of Lion 18650 batteries (18-21.6v 2600mah per cell). I am looking into using USB-C interface (20v 5A 100w) to power the load as well as charging the batteries. And I found this evaluation board from TI, USB-PD-CHG-EVM-01. It seems like what I need but only support up to 4 cells. Do you have a updated design on this with higher cell number support? And if not, is there any DC/DC boost converter recommended for boosting the output load voltage to 54v?
A few specifications regarding my design:
- Max output power 100w
- Max input power 100w
- Battery: 5-6s Lion 18650 batteries (18-21.6v 2600mah per cell)
- Power Path for charging while using
- USB-C charger: 100w 20v 5A
- Battery could power the system without having a USB-C charger plugged in (Is this the OTG function? Correct me if I am wrong.)
Kind regards,
Roy