Hi team,
I have two questions for TPS25810-Q1 as below. Could you advise?
#1. Is there strict requirement for input capacitance?
Input capacitance in Datasheet Figure 20 is 47uF x3.
In my application, maximum Bus current is 900mA. Is it possible to eliminate the amount of input capacitance?
#2. CC capability broadcast for STD mode in table 3 below.
How much is the maximum load current if STD is selected?
Is that 500mA for USB2.0, 900mA/1.5A for USB3.2?

regards,