I'm trying to find a part that can create -5V capable of supplying 5A. Available system voltages are 24V, 12V, 5V and 3.3V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to find a part that can create -5V capable of supplying 5A. Available system voltages are 24V, 12V, 5V and 3.3V.
Hello Mike,
Normally you can use any step-down converter to generate a negative output voltage. The GND pin of the converter is then floating and the inductor is connected to the system GND. For more details, please review this application note: http://www.ti.com/litv/pdf/slva317a
Best regards,
Brigitte