Part Number: TPS65100
Hello,
I have some problems with the TPS65100.
My display has these requirements:
- AVDD: 10,2V @ 25 mA max.
- VGH: 20V @ 1 mA max.
- VGL: -10V @ 2,5 mA max.
- VCOM: 4.3V @

Initially after a few seconds it went into fault mode, and I understood that the problem was the TPS65100 that was not able to reach the VGL voltage, so I reduced R5 to bring the voltage to -7.5 and so everything worked correctly. There is a mode to achieve -10V?
The second problem always concerns the start-up phase, i.e. if, for example, I leave the board on with the display for many hours it works correctly without ever going into fault, but if I immediately restart the board (remove and reconnect the power supply) the TPS65100 after a few seconds goes into fault. The only way to start it correctly is to cool the TPS65100 part of the circuit (50°C approx).
So it's a temperature problem that only occurs during the start-up phase, but I'm widely below the maximum working temperature declared on the data sheet.
I tried to monitor the various voltages with the oscilloscope and the only strange thing I found was in the SW pin, which during the start-up phase has a strange oscillation that disappears if instead of going into fault it maintains the voltages correctly.
Do you have any possible solution?
Many thanks.