This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: a sudden TrueRemQ change

Part Number: BQ28Z610-R1

Hi,

              below is the gg and log,  please  help to  example while there is a 110mAh change of TrueRemQ, thanks. 

0636.GG+LOG.rar

  • It looks like the gauge detected a full charge (taper current is 800mA and the log file shows that the charging current dropped below this for the required time). When it does this, it will record the voltage and temperature and re-run a discharge simulation. It happened that the charge termination measurements (together with the load prediction for this configuration) resulted in slightly less capacity and hence true RM drops a bit.