Other Parts Discussed in Thread: TPS54361, TPS54360, LM76003
hello TI engineers
I would like to use TPS54360B for make a negative voltage of -15V, with input voltage 24V.
I would like to use TPS54360B as in a buck-boost converter.
My questions are:
1) What is the current sense resistor in TPS54360B?
In my opinion, Rsen = 1/gm_ps = 1 / (12 A/V) = 1/12 ohm. Is this correct?
Reference: SLVAE22A–July 2018–Revised March 2019
2) And what is the slope compensation Se? I didn't find anything about it in the datasheet
In the following reference (family excel tool), it shows Se = 1 A/V
I think Se should have a unit as V/Sec or V/uSec
Can you please give me a better explanation and definition on Se?
Reference:
CALCULATION TOOL, TPS54360 and TPS54361 Family Design Excel Tool (Rev. E), SLVC452E.ZIP (245 KB)
3) Is there any other better solution to create a +24Vin, -15Vout and 1A non-isolated DC-DC converter?
Thanks
Ye