This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2985: LP2985 Disable issue, Vout is 2.0 when disabled.

Part Number: LP2985

LP2985-5.0 enable issue: Vin=5.5Vdc . Vout=5.0 

When nothing connected to the Vout, I see the the Vout=0 when enable is LOW. 

But the Vout is connected to some chips, when Enable=Low, the Vout is 2.0Vdc . Very strange. 

Is the Vout in high impedance state when Enable=low. Wonder what is going on?