Other Parts Discussed in Thread: IWR6843ISK, , LP87702
Hello,
we used the the LP87702DRHBRQ1 in our Projekt to manage the power supply for our IWR6843ISK Board.
Due to availability issues of the of the LP87702DRHBRQ1 we were considering, using the LP87702KRHBR.
As far as i understand, the only difference of these is the OTP-Memory which leads to a 1V output at Buck Converter 1 instead of 1.24V. Apart from this, it is the same chip.
Is it a valid workaround, to add a series resistance to the feedback input 1 to adjust the voltage of the LP87702KRHBR Buck Converter to 1.24V?


Thanks and greetings
Robert Schmidt