Other Parts Discussed in Thread: TPS7A53-Q1
Dear team,
Could you suggest P2P LDO solution for TPS7A5401QRGRRQ1?
non-Q grade/ BoM change/ similar function are acceptable.
We want to build 2nd source for this part.
Regards,
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
Could you suggest P2P LDO solution for TPS7A5401QRGRRQ1?
non-Q grade/ BoM change/ similar function are acceptable.
We want to build 2nd source for this part.
Regards,
Ben
Hi Ben,
I can get back to you on this by EOD tomorrow.
Regards,
Kelsey
Hi Ben,
TPS7A5301QRGRRQ1 is p2p; it is the 3A-rated version in this family of devices. If the full 4A isn't necessary, this is the alternate device I would recommend for 2nd sourcing.
Please find the comparison table between the two devices below:
| TPS7A5401QRGRRQ1 | TPS7A5301QRGRRQ1 | |
| Generic Part Number | TPS7A54-Q1 | TPS7A53-Q1 |
| Iout(Max)(A) | 4 | 3 |
| Vin(Max)(V) | 6.5 | 6.5 |
| Vin(Min)(V) | 1.1 | 1.1 |
| Vout(Max)(V) | 5.1 | 5.15 |
| Vout(Min)(V) | 0.8 | 0.8 |
| Fixed Voltage(V) | ADJ | ADJ |
| PSRR @ 100 KHz(dB) |
33 | 39 |
| Noise(uVrms) | 4.4 | 4.4 |
| Accuracy(%) | 1 | 1 |
| Dropout voltage (Vdo)(Typ)(mV) |
150 | 110 |
| Iq(Typ) (mA) |
3 | 3 |
| Output capacitor type | Ceramic | Ceramic |
| Thermal resistance θJA(°C/W) |
40 | 40 |
| Operating temperature range(C) |
-40 to 150 | -40 to 150 |
| Package size: mm2 | 12 mm2: 3.5 x 3.5 (VQFN|20) | 12 mm2: 3.5 x 3.5 (VQFN|20), 16 mm2: 4 x 4 (VQFN|20) |
| Package | VQFN|20 | VQFN|20 |
| Pin 1 | OUT | OUT |
| Pin 2 | NC | NC |
| Pin 3 | FB | FB |
| Pin 4 | PG | PG |
| Pin 5 | DNC | DNC |
| Pin 6 | NC | NC |
| Pin 7 | NC | NC |
| Pin 8 | GND | GND |
| Pin 9 | NC | NC |
| Pin 10 | NC | NC |
| Pin 11 | NC | NC |
| Pin 12 | BIAS | BIAS |
| Pin 13 | NR/SS | NR/SS |
| Pin 14 | EN | EN |
| Pin 15 | IN | IN |
| Pin 16 | IN | IN |
| Pin 17 | IN | IN |
| Pin 18 | GND | GND |
| Pin 19 | OUT | OUT |
| Pin 20 | OUT | OUT |
Regards,
Kelsey