Other Parts Discussed in Thread: SM72445,
Dear Experts,
I am designing a solar charger with SM72445 that charges 48V batteries. The input range of the solar cells varies from 30V to 180V so it means that
1:1 (100% duty cycle) can happen when the input is around the output charging voltage (2% variation based on the datasheet of the SM72445).
The question is that how the SM72445 will toggle the output low side switch mosfets in 100% to keep the two high side mosfets on during this bypass mode?
I am asking this question because UCC27712 drivers can work in 100% duty cycle but the control has to make sure that the low side fets are toggled
with a certain frequency so the bootstrap supply (Voltage on HB-HS) of the high side nmos driver recharges periodically and does not fall below uvlo.
Thanks and regards,
Andras