The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

If ADI LTC3833IFE#PBF have TI P2P device?

Other Parts Discussed in Thread: LM5149

Hi E2E,

If TI have ADI LTC3833IFE#PBF (TSSOP-24 4.5V-38V 20A.Linear) P2P device? 

Project Name: COS-2507
Customer: TXONE
End customer Name: by NDA
Application: SEVER
Usage: network interface card
MP schedule: 2023 Q1

Thank you.

  • Hi,

    There is no pin-to-pin TI buck controller device that is compatible with the LTC3833 (20 pin QFN or TSSOP).

    If customer is interested in a new controller device than the newly released LM5149 would be recommended. However this will require a redesign of the board. 

    Regards,

    Jimmy