The bq35100 is used in the company's main product to measure the consumed uAh in active mode. The ACCUMULATOR mode is used. We have a device that has written to the flash approximately 90.0000 times; the last accumulated capacity read is 4262200296 = FE0C 03E8.
We checked the status register on the bq35100 and found a value of 0x2081 = 0010 0000 1000 0001. Bit 15 is set to zero, indicating that the device has NOT detected a failed write to data flash.
It is worth noting that in our case, the AccumulatedCapacity register was observed to count down from FFFF FFFF to 0 (in our case the min reach was FE0C 03E8). According to the datasheet, the accumulator rises from 0 to 4.29E9 and does not roll over when full.