What is the possible way to bring the device out of the discharge cut in case of OCD1 as the document say that the charging current can only bring it out. But usually, in general load removal works as a recovery model for the same. So how can i configure it so that it detects load removal and comes out of the discharge cut.
Also, what is the configuration for OCC , for example we are setting OCC threshold at 10mV but the OCC cut is coming up on 12A and 4mV for 4A but since we have the unit of 2mV so why it is not working accordingly and we cannot see the safety alert on the GUI for the same.
Also help me with the internal balancing configuration because i am not able to check it in charging condition only.