Hello,
I ran a simulation with LTspice using a PSpice model of TPS70950 provided by TI.
I want to use this regulator with floating ground, so I used square-wave voltage source as the ground.
The schematic is as follows.
As a result of the simulation, the output voltage Vout is about the reversed ground voltage.
This output voltage does not change when changing the input voltage.
When the ground is connected to constant 0V source, the output voltage was 5V as the following figure. So, it worked well when the ground is not floating.
When I used LT1086-5 as a regulator with floating ground, it worked well as follows.
I want to know if TPS70950 can be used for applications with a floating ground.
If there is any mistake in my schematic, please tell me.