Hi,
Customer did a test on TPS2061C:
- Add 500mA load from electronical load.
- Short Vout to GND.
- Remove Short, but 500mA load is still added. Vout cannot have 5V output, only 1.2V around.
- Remove DC load, Vout has 5V output.
Question is how to make Vout has 5V output even 500mA load added at step 3. this is supposed 2 USB ports are used, 1 port is short, and 1 port offer 500mA to device normally. when SCP is removed, the port should work normally Vout = 5V. what can we do to make it?
CH1 yellow: OC#
CH3 Pink: VIN
CH4 Green: Vout